NXOpen.UF.Path.Cutcom Structure¶
NXOpen.UF.Path.Cutcom is an alias for NXOpen.UF.PathCutcom_Struct
-
class
NXOpen.UF.
PathCutcom_Struct
¶ Bases:
object
Refer to UF_PATH_cutcom_s for documentation.
Fields
NXOpen.UF.PathCutcom_Struct.CutcomMode |
*********************************************************************** Specify data for the CUTCOM/ post command. ************************************************************************ |
NXOpen.UF.PathCutcom_Struct.PlaneType |
|
NXOpen.UF.PathCutcom_Struct.CutcomOnStatus |
|
NXOpen.UF.PathCutcom_Struct.CutcomOffStatus |
|
NXOpen.UF.PathCutcom_Struct.AdjustRegister |
the register to use for cutter compensation |
NXOpen.UF.PathCutcom_Struct.FullCutcomOutput |
a full cutcom command is output if and only if this fl ag is TRUE. |
NXOpen.UF.PathCutcom_Struct.AdjustFlag |
the adjust register is output if and only if this flag is TRUE. |