NXOpen.UF.Path.CreateSeqno¶
-
Path.
CreateSeqno
()¶ Refer to UF_PATH_create_seqno for documentation.
Signature:
CreateSeqno(pathId, seqType, seqNumber, seqIncr, seqFreq, text)
Parameters: - pathId (PointerWrapper) – The path id for this event
- seqType (
NXOpen.UF.Path.Seqno
Refer to UF_PATH_seqno_e for documentation.) – The sequence type - seqNumber (int) – The sequence number, only valid if seq_type is UF_PATH_SEQNO_N
- seqIncr (int) – Only valid if seq_type is UF_PATH_SEQNO_N
- seqFreq (int) – Only valid if seq_type is UF_PATH_SEQNO_N
- text (str) – The post command appended text
License requirements: None