NXOpen.UF.Part.OpenQuiet¶
-
Part.
OpenQuiet
()¶ Refer to UF_PART_open_quiet for documentation.
Signature:
OpenQuiet(partName)
Parameters: partName (str) – Name of part to retrieve. Returns: A Tuple Return type: A tuple consisting of (part,errorStatus) part(Tag): The tag of the retrieved part or NULL_TAG if part retrieval fails.
errorStatus(
`NXOpen.UF.Part.LoadStatus
Refer to UF_PART_load_status_s for documentation.`): The user allocated structure is filled with the names and associated error codes of any parts that did not load correctly. The structure must be freed with UF_PART_free_load_status. For details see the definition of UF_PART_load_status_t.License requirements: None