NXOpen.UF.Part.OpenCset¶
-
Part.
OpenCset
()¶ Refer to UF_PART_open_cset for documentation.
Signature:
OpenCset(cset)
Parameters: cset (Tag) – set of components to open Returns: The user allocated structure is filled with the names and associated error codes of any parts that did not load correctly. The structure must be freed with UF_PART_free_load_status. For details see the definition of UF_PART_load_status_t. Return type: NXOpen.UF.Part.LoadStatus
Refer to UF_PART_load_status_s for documentation.License requirements: None