NXOpen.UF.Part.Import¶
-
Part.
Import
()¶ Refer to UF_PART_import for documentation.
Signature:
Import(fileName, modes, destCsys, destPoint, scale)
Parameters: - fileName (str) – File specification of NX disk file to import.
- modes (
NXOpen.UF.Part.ImportPartModes
Refer to UF_import_part_modes_s for documentation.) – Inputs are specified in the `modes’ structure. - destCsys (list of float) – Destination Coordinate System. dest_csys[0..2] is an X-direction vector, and dest_csys[3..5] is a y direction vector. These are used as input to UF_MTX3_initialize to create the full coordinate system matrix.
- destPoint (list of float) – Destination point of imported part
- scale (float) – The scale size for the imported part.
Returns: If grouping is desired, the group is returned, otherwise it is a NULL_TAG
Return type: License requirements: None