NXOpen.UF.Oper.AskSelectedPointData¶
-
Oper.
AskSelectedPointData
()¶ Refer to UF_OPER_ask_selected_point_data for documentation.
Signature:
AskSelectedPointData(objectTag, index)
Parameters: - objectTag (Tag) – the tag of the operation of the points
- index (int) – index of tracking point in parent (from 0 to the number of selected points - 1)
Returns: the data of the point
Return type: NXOpen.UF.Cutter.TrackingPointData
Refer to UF_CUTTER_tracking_point_data_s for documentation.License requirements: None