NXOpen.UF.Motion.ScalarForceTorque Structure¶
NXOpen.UF.Motion.ScalarForceTorque is an alias for NXOpen.UF.MotionScalarForceTorque_Struct
-
class
NXOpen.UF.
MotionScalarForceTorque_Struct
¶ Bases:
object
Refer to UF_MOTION_scalar_force_torque_s for documentation.
Fields
NXOpen.UF.MotionScalarForceTorque_Struct.Name |
The name of the force or torque. |
NXOpen.UF.MotionScalarForceTorque_Struct.AttachBody |
The link the force is acting on, or the revolute joint the torque is acting on. |
NXOpen.UF.MotionScalarForceTorque_Struct.Origin1 |
The point that defines the location the force is acting from. |
NXOpen.UF.MotionScalarForceTorque_Struct.Origin2 |
The point that defines the location the force is acting to. |
NXOpen.UF.MotionScalarForceTorque_Struct.ForceFunction |
The function describing the force magnitude. |
NXOpen.UF.MotionScalarForceTorque_Struct.TorqueFunction |
The function describing the torque magnitude. |
NXOpen.UF.MotionScalarForceTorque_Struct.ReactionLink |
The optional link that receives an equal and opposite reaction force. |