NXOpen.UF.Motion.PointOnSurfaceData Structure¶
NXOpen.UF.Motion.PointOnSurfaceData is an alias for NXOpen.UF.MotionPointOnSurfaceData_Struct
-
class
NXOpen.UF.
MotionPointOnSurfaceData_Struct
¶ Bases:
object
Refer to UF_MOTION_point_on_surface_data_s for documentation.
Fields
NXOpen.UF.MotionPointOnSurfaceData_Struct.PointOnSurfaceTag |
Tag of the created/edited entity |
NXOpen.UF.MotionPointOnSurfaceData_Struct.PointTag |
The point tag of the point on surface constraint. |
NXOpen.UF.MotionPointOnSurfaceData_Struct.PointLinkTag |
Optional: The user need not specify this data. |
NXOpen.UF.MotionPointOnSurfaceData_Struct.NumFaceTags |
Number of face tags for the constraint |
NXOpen.UF.MotionPointOnSurfaceData_Struct.FaceTags |
Group of faces that can be have a parameterized UV space. |
NXOpen.UF.MotionPointOnSurfaceData_Struct.FaceLinkTag |
Optional: The user need not specify this data. |
NXOpen.UF.MotionPointOnSurfaceData_Struct.DisplayScale |
This scale is used in UI for displaying the object |
NXOpen.UF.MotionPointOnSurfaceData_Struct.EntityName |
A unique name for the object |