NXOpen.UF.Motion.Marker Structure¶
NXOpen.UF.Motion.Marker is an alias for NXOpen.UF.MotionMarker_Struct
-
class
NXOpen.UF.
MotionMarker_Struct
¶ Bases:
object
Refer to UF_MOTION_marker_s for documentation.
Fields
NXOpen.UF.MotionMarker_Struct.Name |
The name of the marker. |
NXOpen.UF.MotionMarker_Struct.MarkerType |
Type of marker. |
NXOpen.UF.MotionMarker_Struct.AttachmentTag |
The mechanism object that this marker is attached to. |
NXOpen.UF.MotionMarker_Struct.OrientationTag |
Orientation matrix that defines the orientation of the marker. |
NXOpen.UF.MotionMarker_Struct.OriginTag |
Smart point that defines the origin of the marker. |
NXOpen.UF.MotionMarker_Struct.Location |
Coordinates that define the location of the marker. |