NXOpen.UF.Motion.LinkMassProperties Structure¶
NXOpen.UF.Motion.LinkMassProperties is an alias for NXOpen.UF.MotionLinkMassProperties_Struct
-
class
NXOpen.UF.
MotionLinkMassProperties_Struct
¶ Bases:
object
Refer to UF_MOTION_link_mass_properties_s for documentation.
Fields
NXOpen.UF.MotionLinkMassProperties_Struct.MassCenter |
Smart point at the center of mass. |
NXOpen.UF.MotionLinkMassProperties_Struct.InertiaMarker |
Internal marker that defines the origin and orientation of the inertia values. |
NXOpen.UF.MotionLinkMassProperties_Struct.Mass |
The mass of the link |
NXOpen.UF.MotionLinkMassProperties_Struct.ProductsOfInertia |
The products of inertia of the link in the following order: Ixx, Ixy, Ixz, Iyy, Iyz, Iyz |
NXOpen.UF.MotionLinkMassProperties_Struct.UserDefined |
TRUE if overriding default mass properties with user defined values. |