NXOpen.UF.Motion.Joint Structure¶
NXOpen.UF.Motion.Joint is an alias for NXOpen.UF.MotionJoint_Struct
-
class
NXOpen.UF.
MotionJoint_Struct
¶ Bases:
object
Refer to UF_MOTION_joint_s for documentation.
Fields
NXOpen.UF.MotionJoint_Struct.Name |
The name of the joint. |
NXOpen.UF.MotionJoint_Struct.JtType |
The type of the joint. |
NXOpen.UF.MotionJoint_Struct.SnapLinks |
If TRUE, the joint “snaps” the two links into position using the link orientations. |
NXOpen.UF.MotionJoint_Struct.Link1 |
The first link associated with the joint. |
NXOpen.UF.MotionJoint_Struct.Link2 |
The second link associated with the joint. |
NXOpen.UF.MotionJoint_Struct.Direction1 |
Smart direction tag that defines the direction of link_1. |
NXOpen.UF.MotionJoint_Struct.Direction2 |
Smart direction tag that defines the direction of link_2. |
NXOpen.UF.MotionJoint_Struct.Origin1 |
Optional point location on link_1. |
NXOpen.UF.MotionJoint_Struct.Origin2 |
Optional point location on link_2. |
NXOpen.UF.MotionJoint_Struct.ScrewRatio |
Used only for UF_MOTION_screw_joint. |