NXOpen.UF.MotionJointMotionInput_Struct.HarmDisp¶
-
MotionJointMotionInput_Struct.
HarmDisp
¶ The harmonic offset displacement input. This is the distance from the design position to the center of the harmonic wave. If the wave is to be centered at the design position, this value should be zero. Used if type is UF_MOTION_harmonic_input.