NXOpen.UF.Motion.GeneralBushing Structure¶
NXOpen.UF.Motion.GeneralBushing is an alias for NXOpen.UF.MotionGeneralBushing_Struct
-
class
NXOpen.UF.
MotionGeneralBushing_Struct
¶ Bases:
object
Refer to UF_MOTION_general_bushing_s for documentation.
Fields
NXOpen.UF.MotionGeneralBushing_Struct.Name |
The name of the bushing. |
NXOpen.UF.MotionGeneralBushing_Struct.Link1 |
The first link of the bushing. |
NXOpen.UF.MotionGeneralBushing_Struct.Origin1 |
The point that defines the location of the bushing on link_1. |
NXOpen.UF.MotionGeneralBushing_Struct.Direction1 |
The direction vector that defines the orientation of the bushing on link_1. |
NXOpen.UF.MotionGeneralBushing_Struct.Link2 |
The second link of the bushing or NULL_TAG to attach to ground. |
NXOpen.UF.MotionGeneralBushing_Struct.Origin2 |
The point that defines the location of the bushing on link_2, or NULL_TAG if ground. |
NXOpen.UF.MotionGeneralBushing_Struct.Direction2 |
The direction vector that defines the orientation of the bushing on link_2, or NULL_TAG if ground. |
NXOpen.UF.MotionGeneralBushing_Struct.TranslationalStiffness |
The x, y, and z components of the translational stiffness with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionGeneralBushing_Struct.TranslationalDamping |
The x, y, and z components of the translational damping with respect to the bushing orientatation on link_1. |
NXOpen.UF.MotionGeneralBushing_Struct.TranslationalPreload |
The x, y, and z components of the translational preload with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionGeneralBushing_Struct.TorsionalStiffness |
The x, y, and z components of the torsional stiffness with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionGeneralBushing_Struct.TorsionalDamping |
The x, y, and z components of the torsional damping with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionGeneralBushing_Struct.TorsionalPreload |
The x, y, and z components of the torsional preload with respect to the bushing orientation on link_1. |