NXOpen.UF.Motion.CylindricalBushing Structure¶
NXOpen.UF.Motion.CylindricalBushing is an alias for NXOpen.UF.MotionCylindricalBushing_Struct
-
class
NXOpen.UF.
MotionCylindricalBushing_Struct
¶ Bases:
object
Refer to UF_MOTION_cylindrical_bushing_s for documentation.
Fields
NXOpen.UF.MotionCylindricalBushing_Struct.Name |
The name of the bushing. |
NXOpen.UF.MotionCylindricalBushing_Struct.Link1 |
The first link of the bushing. |
NXOpen.UF.MotionCylindricalBushing_Struct.Origin1 |
The point that defines the location of the bushing on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.Direction1 |
The direction vector that defines the orientation of the bushing on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.Link2 |
The second link of the bushing or NULL_TAG to attach to ground. |
NXOpen.UF.MotionCylindricalBushing_Struct.Origin2 |
The point that defines the location of the bushing on link_2, or NULL_TAG if ground. |
NXOpen.UF.MotionCylindricalBushing_Struct.Direction2 |
The direction vector that defines the orientation of the bushing on link_2, or NULL_TAG if ground. |
NXOpen.UF.MotionCylindricalBushing_Struct.RadialStiffness |
The radial stiffness with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.LongitudinalStiffness |
The longitudinal stiffness with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.ConicalStiffness |
The conical stiffness with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.TorsionalStiffness |
The torsional stiffness with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.RadialDamping |
The radial damping with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.LongitudinalDamping |
The longitudinal damping with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.ConicalDamping |
The conical damping with respect to the bushing orientation on link_1. |
NXOpen.UF.MotionCylindricalBushing_Struct.TorsionalDamping |
The torsional damping with respect to the bushing orientation on link_1. |