NXOpen.UF.Motion.CurveCurveConstraint Structure¶
NXOpen.UF.Motion.CurveCurveConstraint is an alias for NXOpen.UF.MotionCurveCurveConstraint_Struct
-
class
NXOpen.UF.
MotionCurveCurveConstraint_Struct
¶ Bases:
object
Refer to UF_MOTION_curve_curve_constraint_s for documentation.
Fields
NXOpen.UF.MotionCurveCurveConstraint_Struct.Name |
The name of the curve curve constraint. |
NXOpen.UF.MotionCurveCurveConstraint_Struct.NumCurve1Tags |
The number of tags in the first curve tag array. |
NXOpen.UF.MotionCurveCurveConstraint_Struct.Curve1 |
The tags of the first constraint curves. |
NXOpen.UF.MotionCurveCurveConstraint_Struct.NumCurve2Tags |
The number of tags in the second curve tag array. |
NXOpen.UF.MotionCurveCurveConstraint_Struct.Curve2 |
The tags of the second constraint curves. |