NXOpen.UF.Motion.TraceModel¶
-
Motion.
TraceModel
()¶ Refer to UF_MOTION_trace_model for documentation.
Signature:
TraceModel(stepNum, targetLayer)
Parameters: - stepNum (int) – The step number of the current analysis solution in the database. It cannot be negative and it cannot exceed the number of valid steps in the solution.
- targetLayer (int) – The layer to place the new objects on. It must be a valid NX layer.
Returns: A Tuple
Return type: A tuple consisting of (numTags,geomTags)
numTags(int): The number of geometry tags copied and returned in the next argument.
geomTags(list of Tag): The tags of the copied geometry of all the links. The memory for this array of tags must be freed using UF_free().
License requirements: None