NXOpen.UF.Motion.SpreadsheetRunFromFile¶
-
Motion.
SpreadsheetRunFromFile
()¶ Refer to UF_MOTION_spreadsheet_run_from_file for documentation.
Signature:
SpreadsheetRunFromFile(spreadsheetFile, startStep, endStep, invokeUi)
Parameters: - spreadsheetFile (str) – Full path and name of spreadsheet filecontaining motion data
- startStep (int) – Step number in spreadsheet to startanimation at
- endStep (int) – Step number in spreasheet till which toanimate
- invokeUi (bool) – TRUE if spreadsheet run should be interactive FALSE if animation should be run without the user interface
License requirements: None