NXOpen.UF.Motion.SetSpring¶
-
Motion.
SetSpring
()¶ Refer to UF_MOTION_set_spring for documentation.
Signature:
SetSpring(springTag, springStruct)
Parameters: - springTag (Tag) – The tag of the spring to set. This tag is the one returned from the UF_MOTION_create_spring function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type)
- springStruct (
NXOpen.UF.Motion.SpringDamper
Refer to UF_MOTION_spring_damper_s for documentation.) – The spring structure for the input tag.
License requirements: None