NXOpen.UF.Motion.SetLinkMassProperties¶
-
Motion.
SetLinkMassProperties
()¶ Refer to UF_MOTION_set_link_mass_properties for documentation.
Signature:
SetLinkMassProperties(linkTag, massPropStruct)
Parameters: - linkTag (Tag) – The tag of the link to set mass properties. This tag is the one returned from the UF_MOTION_create_link function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type)
- massPropStruct (
NXOpen.UF.Motion.LinkMassProperties
Refer to UF_MOTION_link_mass_properties_s for documentation.) – The link mass propertiy structure for the input tag. These mass properties will overwrite the mass properties that may have been created automatically for the link.
License requirements: None