NXOpen.UF.Motion.SetJointMotionInput¶
-
Motion.
SetJointMotionInput
()¶ Refer to UF_MOTION_set_joint_motion_input for documentation.
Signature:
SetJointMotionInput(jointTag, inputStruct)
Parameters: - jointTag (Tag) – The tag of the joint to set the motion input info to. This tag must belong to either a revolute or a slider joint. This tag is the one returned from the UF_MOTION_create_joint function. It can also be found using object cycle functions (eg. UF_OBJ_cycle_objs_by_type).
- inputStruct (
NXOpen.UF.Motion.JointMotionInput
Refer to UF_MOTION_joint_motion_input_s for documentation.) – The joint motion input structure to be set on the input joint tag.
License requirements: None