NXOpen.UF.Motion.AskVectorForceTorque¶
-
Motion.
AskVectorForceTorque
()¶ Refer to UF_MOTION_ask_vector_force_torque for documentation.
Signature:
AskVectorForceTorque(vobjectTag)
Parameters: vobjectTag (Tag) – The tag of the vector force or torque to return information about. This tag is the one returned from UF_MOTION_create_vector_force_torque. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The vector force/ torque structure for the input tag. Return type: NXOpen.UF.Motion.VectorForceTorque
Refer to UF_MOTION_vector_force_torque_s for documentation.License requirements: None