NXOpen.UF.Motion.AskScalarForce¶
-
Motion.
AskScalarForce
()¶ Refer to UF_MOTION_ask_scalar_force for documentation.
Signature:
AskScalarForce(forceTag)
Parameters: forceTag (Tag) – The tag of the scalar force to return information about. This tag is the one returned from UF_MOTION_create_scalar_force. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The scalar force structure for the input tag. Return type: NXOpen.UF.Motion.ScalarForceTorque
Refer to UF_MOTION_scalar_force_torque_s for documentation.License requirements: None