NXOpen.UF.Motion.AskRotDisplacementResults¶
-
Motion.
AskRotDisplacementResults
()¶ Refer to UF_MOTION_ask_rot_displacement_results for documentation.
Signature:
AskRotDisplacementResults(motionObject, component, refFrame)
Parameters: - motionObject (Tag) – The tag of the object to get the results for. This is usually a joint, constraint, coupler, marker, or primitive.
- component (
NXOpen.UF.Motion.DispAngle
Refer to UF_MOTION_disp_angle_e for documentation.) – The desired displacement angle. This can be the Euler angles that follow the body 3-1-3 convention. See the enum definition for more information. - refFrame (
NXOpen.UF.Motion.ReferenceFrame
Refer to UF_MOTION_reference_frame_e for documentation.) – The reference frame that the results will be resolved in (Example: UF_MOTION_absolute).
Returns: A Tuple
Return type: A tuple consisting of (numberOfResults,results)
numberOfResults(int): The number of results returned in the next argument. This will equal the number of steps in the solution.
results(list of float): The results requested. This array must be freed by the calling function using UF_free().
License requirements: None