NXOpen.UF.Motion.AskMeasurement¶
-
Motion.
AskMeasurement
()¶ Refer to UF_MOTION_ask_measurement for documentation.
Signature:
AskMeasurement(measTag)
Parameters: measTag (Tag) – The tag of the measurement to return. This tag is the one returned from the creation function (UF_MOTION_create_measurement). It can also be found using object cycle functions (eg. UF_OBJ_cycle_objs_by_type). Returns: The measurement structure for the input tag. Return type: NXOpen.UF.Motion.Measurement
Refer to UF_MOTION_measurement_s for documentation.License requirements: None