NXOpen.UF.Motion.AskJointMotionInput¶
-
Motion.
AskJointMotionInput
()¶ Refer to UF_MOTION_ask_joint_motion_input for documentation.
Signature:
AskJointMotionInput(jointTag)
Parameters: jointTag (Tag) – The tag of the joint to return the motion input info of. This tag is the one returned from the UF_MOTION_create_joint function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The joint motion input structure for the input joint tag. Return type: NXOpen.UF.Motion.JointMotionInput
Refer to UF_MOTION_joint_motion_input_s for documentation.License requirements: None