NXOpen.UF.Motion.AskJointCoupler¶
-
Motion.
AskJointCoupler
()¶ Refer to UF_MOTION_ask_joint_coupler for documentation.
Signature:
AskJointCoupler(jointCouplerTag)
Parameters: jointCouplerTag (Tag) – The tag of the joint coupler to return. This tag is the one returned from the UF_MOTION_create_joint_coupler function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The joint coupler structure for the input joint coupler tag. Return type: NXOpen.UF.Motion.JointCoupler
Refer to UF_MOTION_joint_coupler_s for documentation.License requirements: None