NXOpen.UF.Motion.AskJoint¶
-
Motion.
AskJoint
()¶ Refer to UF_MOTION_ask_joint for documentation.
Signature:
AskJoint(jointTag)
Parameters: jointTag (Tag) – The tag of the joint to return information about. This tag is the one returned from the UF_MOTION_create_joint function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The joint structure for the input tag. Return type: NXOpen.UF.Motion.Joint
Refer to UF_MOTION_joint_s for documentation.License requirements: None