NXOpen.UF.Motion.AskInterference¶
-
Motion.
AskInterference
()¶ Refer to UF_MOTION_ask_interference for documentation.
Signature:
AskInterference(interfereTag)
Parameters: interfereTag (Tag) – The tag of the interference to return. This tag is the one returned from the UF_MOTION_create_interference function. It can also be found using object cycle functions (eg. UF_OBJ_cycle_objs_by_type). Returns: The interference structure for the input tag. Return type: NXOpen.UF.Motion.Interference
Refer to UF_MOTION_interference_s for documentation.License requirements: None