NXOpen.UF.Motion.AskGeneralBushing¶
-
Motion.
AskGeneralBushing
()¶ Refer to UF_MOTION_ask_general_bushing for documentation.
Signature:
AskGeneralBushing(bushingTag)
Parameters: bushingTag (Tag) – The tag of the general bushing to return information about. This tag is the one returned from the UF_MOTION_create_general_bushing function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The general bushing structure for the input tag. Return type: NXOpen.UF.Motion.GeneralBushing
Refer to UF_MOTION_general_bushing_s for documentation.License requirements: None