NXOpen.UF.Motion.AskDamper¶
-
Motion.
AskDamper
()¶ Refer to UF_MOTION_ask_damper for documentation.
Signature:
AskDamper(damperTag)
Parameters: damperTag (Tag) – The tag of the damper to return information about. This tag is the one returned from the UF_MOTION_create_damper function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The damper structure for the input tag. Return type: NXOpen.UF.Motion.SpringDamper
Refer to UF_MOTION_spring_damper_s for documentation.License requirements: None