NXOpen.UF.Motion.AskCylindricalBushing¶
-
Motion.
AskCylindricalBushing
()¶ Refer to UF_MOTION_ask_cylindrical_bushing for documentation.
Signature:
AskCylindricalBushing(bushingTag)
Parameters: bushingTag (Tag) – The tag of the cylindrical bushing to return information about. This tag is the one returned from the UF_MOTION_create_cylindrical_bushing function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The cylindrical bushing structure for the input tag. Return type: NXOpen.UF.Motion.CylindricalBushing
Refer to UF_MOTION_cylindrical_bushing_s for documentation.License requirements: None