NXOpen.UF.Motion.AskCrvCrvConstraint¶
-
Motion.
AskCrvCrvConstraint
()¶ Refer to UF_MOTION_ask_crv_crv_constraint for documentation.
Signature:
AskCrvCrvConstraint(crvCrvTag)
Parameters: crvCrvTag (Tag) – The tag of the constraint to return. This tag is the one returned from the UF_MOTION_create_crv_crv_constraint function. It can also be found using object cycle functions. (eg. UF_OBJ_cycle_objs_by_type) Returns: The curve-curve structure for the input tag. Return type: NXOpen.UF.Motion.CurveCurveConstraint
Refer to UF_MOTION_curve_curve_constraint_s for documentation.License requirements: None