NXOpen.UF.Motion.AskArticStepSize¶
-
Motion.
AskArticStepSize
()¶ Refer to UF_MOTION_ask_artic_step_size for documentation.
Signature:
AskArticStepSize(jointTag)
Parameters: jointTag (Tag) – The tag of the joint to return the step size for. This tag is returned from the function UF_MOTION_create_joint. It can also be found using object cycle functions (eg. UF_OBJ_cycle_objs_by_type). Returns: The size of the articulation joint step. The units of the step are based on the units of the joint. Return type: float License requirements: None