NXOpen.UF.Modl.WrapGeom Structure¶
NXOpen.UF.Modl.WrapGeom is an alias for NXOpen.UF.ModlWrapGeom_Struct
-
class
NXOpen.UF.
ModlWrapGeom_Struct
¶ Bases:
object
Refer to UF_MODL_wrap_geom_s for documentation.
Fields
NXOpen.UF.ModlWrapGeom_Struct.CloseGap |
Method used to close gaps between faces after offsetting them. |
NXOpen.UF.ModlWrapGeom_Struct.DistTol |
Tolerance used to generate vertices from geometry. |
NXOpen.UF.ModlWrapGeom_Struct.AddOffset |
Additional offset applied to faces. |
NXOpen.UF.ModlWrapGeom_Struct.SplitOffset |
Offset applied to each side of the splitting plane so that the resulting bodies overlap and can be united. |
NXOpen.UF.ModlWrapGeom_Struct.NumGeoms |
Number of tags in the geometry array. |
NXOpen.UF.ModlWrapGeom_Struct.Geometry |
Array of geometry tags. |
NXOpen.UF.ModlWrapGeom_Struct.NumSplits |
Number of tags in the splits array. |
NXOpen.UF.ModlWrapGeom_Struct.Splits |
Array of smart planes (xforms) and/or datum planes to be used to split the geometry. |