NXOpen.UF.Modl.SnipsrfFeatureData Structure¶
NXOpen.UF.Modl.SnipsrfFeatureData is an alias for NXOpen.UF.ModlSnipsrfFeatureData_Struct
-
class
NXOpen.UF.
ModlSnipsrfFeatureData_Struct
¶ Bases:
object
Refer to UF_MODL_snipsrf_feature_data_s for documentation.
Fields
NXOpen.UF.ModlSnipsrfFeatureData_Struct.EditFace |
NX eid of a face to be snipped |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.BoundaryType |
Snipping bounding object type |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.SnipCvString |
Profile defining the snip curve |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.SnippingPlane |
NX eid of plane used as snipping object, Used only if boundary_type is, UF_MODL_snipsurf_boundary_type_plane |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.ProjectVector |
Projection vector, Necessary only if boundary_type is, UF_MODL_snipsurf_boundary_type_curves |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.SnipOrDivide |
Flag indicating snipping or divide operation, 0: Divide, otherwise Snipping operation Does not play any role during snip surface feature editing |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.RegionPointUv |
Region point on the edit_face indicating the retained side of the face divided by imprinted snipping curve. |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.ProjectMethod |
Project methods:0- along surface normal, 1- along view direction, 2- along x direction, 3- along y direction, 4- along z direction, 5- along given vector |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.RefitMethod |
Surface refitting method |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.RefitDegree |
Refit direction degree, Necessary if refit_type is, UF_MODL_snipsurf_refit_method_deg_patch or UF_MODL_snipsurf_refit_method_deg_tol |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.RefitPatches |
Refit direction patches, Necessary if refit_type is, UF_MODL_snipsurf_refit_method_deg_patch or UF_MODL_snipsurf_refit_method_patch_tol |
NXOpen.UF.ModlSnipsrfFeatureData_Struct.Tols |
Tolerance used for refitting, Necessary if refit_type is, UF_MODL_snipsurf_refit_method_deg_tol or UF_MODL_snipsurf_refit_method_patch_tol |