NXOpen.UF.Modl.SmreliefData Structure¶
NXOpen.UF.Modl.SmreliefData is an alias for NXOpen.UF.ModlSmreliefData_Struct
-
class
NXOpen.UF.
ModlSmreliefData_Struct
¶ Bases:
object
Refer to UF_MODL_smrelief_data_s for documentation.
Fields
NXOpen.UF.ModlSmreliefData_Struct.BaseFace |
Planar face or any face of a flange |
NXOpen.UF.ModlSmreliefData_Struct.FirstCornerEdges |
Edges defining the first corner, should be in the plane of the base face, These edges must intersect. |
NXOpen.UF.ModlSmreliefData_Struct.SecondCornerEdges |
Edges defining the second corner, should be in the plane of the base face, these edges must intersect |
NXOpen.UF.ModlSmreliefData_Struct.OffsetCorner |
Edges defining the third corner, should be in the plane of the base face |
NXOpen.UF.ModlSmreliefData_Struct.FirstCornerFilletRadius |
radius value for first corner fillet . This has to be greater than zero |
NXOpen.UF.ModlSmreliefData_Struct.SecondCornerFilletRadius |
radius value for second corner fillet . This value has to be greater than zero |
NXOpen.UF.ModlSmreliefData_Struct.OsCircleRadius |
radius value for offset corner fillet. This value must be greater than zero |
NXOpen.UF.ModlSmreliefData_Struct.OffsetDistance |
distance by which fillet will be offset inside the body from the offset corner . This value must be greater than or equal to zero and less than offset_corner_fillet_ radius |