NXOpen.UF.ModlSmd.CreateSmdFlange¶
-
ModlSmd.
CreateSmdFlange
()¶ Refer to UF_MODL_create_smd_flange for documentation.
Signature:
CreateSmdFlange(attachFace, referenceEdge, position, xdirection, zdirection, flangeData)
Parameters: - attachFace (Tag) – Attachment face of target body.
- referenceEdge (Tag) – Horizontal edge reference of target body. This should lie on the attachment face of the Flange, else an error will be returned.
- position (list of float) – NOT USED. Origin of flange feature will be found automatically.
- xdirection (list of float) – NOT USED. Direction of flange along the width of the bend will be derived automatically.
- zdirection (list of float) – NOT USED. Normal of attachment/link face will be found automatically.
- flangeData (
NXOpen.UF.Modl.FlangeData
Refer to UF_MODL_flange_data_s for documentation.) – Structure which defines the size and shape of the flange feature. This is expanded to include the parameters for Miter and Butt joints also.
Returns: Object identifier of the flange feature.
Return type: License requirements: SHEET METAL DESIGN