NXOpen.UF.ModlSmd.CreateFlange¶
-
ModlSmd.
CreateFlange
()¶ Refer to UF_MODL_create_flange for documentation.
Signature:
CreateFlange(orig, xdir, zdir, face, edge, thick, width, angle, length, radius, taperL, taperR, angTgl, lenTgl, radTgl)
Parameters: - orig (list of float) – Default origin of flange.
- xdir (list of float) – X-direction of flange (across bend.)
- zdir (list of float) – Z-direction, normal to the face.
- face (Tag) – Face to which the flange should attach.
- edge (Tag) – Horizontal edge.
- thick (str) – Thickness expression string (if null, infer from face)
- width (str) – Width expression string (if null, infer from edge)
- angle (str) – Bend angle expression string
- length (str) – Tangent length expression string
- radius (str) – Inside radius of the bend
- taperL (str) – Left taper of flange
- taperR (str) – Right taper of flange
- angTgl (int) – Bend/Include angle switch
- lenTgl (int) – Tangent/Contour length switch
- radTgl (int) – Inside/Outside radius switch
Returns: Object identifier for the flange feature.
Return type: License requirements: SHEET METAL DESIGN