NXOpen.UF.ModlSmcutoutData_Struct.ProjMethod¶
-
ModlSmcutoutData_Struct.
ProjMethod
¶ The method used to determine the projection vector of the outline curves as well as the direction in which the cutout will be punched through the solid body. Can be one of UF_FACE_NORMALS: project along the placement face reverse normal. UF_ALONG_VECTOR: project along a given vector. See proj_vector below. UF_ALONG_DATUM_AXIS: project along a given datum axis. See datum_axis below.