NXOpen.UF.Modl.LinkedExt Structure¶
NXOpen.UF.Modl.LinkedExt is an alias for NXOpen.UF.ModlLinkedExt_Struct
-
class
NXOpen.UF.
ModlLinkedExt_Struct
¶ Bases:
object
Refer to UF_MODL_linked_ext_s for documentation.
Fields
NXOpen.UF.ModlLinkedExt_Struct.NumBodies |
Number of candidate bodies. |
NXOpen.UF.ModlLinkedExt_Struct.Bodies |
Candidate bodies. |
NXOpen.UF.ModlLinkedExt_Struct.Xforms |
Array of xforms. |
NXOpen.UF.ModlLinkedExt_Struct.NumFaces |
Number of tags in the faces array. |
NXOpen.UF.ModlLinkedExt_Struct.Faces |
Array of face tags. |
NXOpen.UF.ModlLinkedExt_Struct.XformIndex |
Array of indices into xforms array, one index for each face. |
NXOpen.UF.ModlLinkedExt_Struct.GroupResults |
Method used to group resulting sheet bodies. |
NXOpen.UF.ModlLinkedExt_Struct.MassProps |
If true, calculate mass properties of all candidate solid bodies. |
NXOpen.UF.ModlLinkedExt_Struct.DeleteOpenings |
If true, any holes in the resulting sheet are closed up; if false they are left. |
NXOpen.UF.ModlLinkedExt_Struct.AtTimestamp |
If true, each linked region updates at a time determined by its creation timestamp. |