NXOpen.UF.ModlGeneral.CreateIsocurve¶
-
ModlGeneral.
CreateIsocurve
()¶ Refer to UF_MODL_create_isocurve for documentation.
Signature:
CreateIsocurve(faceId, uvFlag, parameter, distTol)
Parameters: - faceId (Tag) – The face identifier.
- uvFlag (int) – 1 = create curve along u isoparameter. 2 = create curve along v isoparameter.
- parameter (float) – Parameter at which to create the curve.
- distTol (float) – Tolerance value. The tolerance is only used when the input face is foreign or an offset of a non analytic face.
Returns: A Tuple
Return type: A tuple consisting of (isocurveId,isocurveCnt)
isocurveId(list of Tag): Array of isoparametric curve identifiers. You may get multiple curves if the face is trimmed. The allocated arrays must be freed with UF_free().
isocurveCnt(int): Number of curves created.
License requirements: SOLIDS MODELING or DRAFTING