NXOpen.UF.ModlGeneral.CreateIsoclineCurves¶
-
ModlGeneral.
CreateIsoclineCurves
()¶ Refer to UF_MODL_create_isocline_curves for documentation.
Signature:
CreateIsoclineCurves(faceId, direction, angle, distTol)
Parameters: - faceId (Tag) – The face identifier
- direction (list of float) – Isocline direction (normalized vector)
- angle (float) – Isocline angle (between specified direction and normals of the curves) in degrees. Angle range is from -90 to +90 degrees.
- distTol (float) – Tolerance value. The tolerance is only used when the input face is foreign or an offset of a non analytic face.
Returns: A Tuple
Return type: A tuple consisting of (isocurveId,isocurveCnt)
isocurveId(list of Tag): Array of isocline curve object identifiers. The allocated arrays must be freed with UF_free().
isocurveCnt(int): Number of curves created.
License requirements: SOLIDS MODELING