NXOpen.UF.ModlGeneral.AskPromotionPath¶
-
ModlGeneral.
AskPromotionPath
()¶ Refer to UF_MODL_ask_promotion_path for documentation.
Signature:
AskPromotionPath(promSolid, fullPath)
Parameters: - promSolid (Tag) – Promoted solid body to be queried
- fullPath (bool) – If false, the instance path to the next level promotion is returned. If true, the full instance path across promotion stacks is returned.
Returns: A Tuple
Return type: A tuple consisting of (instancePath,numInstances)
instancePath(list of Tag): The instance path along which the given solid body was promoted. This is an array of instances, which must be freed by calling UF_free.
numInstances(int): Number of instances
License requirements: None