NXOpen.UF.ModlGeneral.AskPointAlongCurve¶
-
ModlGeneral.
AskPointAlongCurve
()¶ Refer to UF_MODL_ask_point_along_curve for documentation.
Signature:
AskPointAlongCurve(point, curve, offset, direction, tolerance)
Parameters: - point (list of float) – Absolute coordinates of the reference point.
- curve (Tag) – Identifier of the selected curve.
- offset (float) – Offset distance from the reference point along the selected curve.
- direction (int) – Direction flag, 1=Same direction as the selected curve. (from start point to end point) -1=Reverse direction of the selected curve (from end point to start point)
- tolerance (float) – Distance tolerance between solid edge and approximated curve.
Returns: Parameter value for the located point on the selected curve.
Return type: float
License requirements: None