NXOpen.UF.ModlGeneral.AskLinearIsetParms¶
-
ModlGeneral.
AskLinearIsetParms
()¶ Refer to UF_MODL_ask_linear_iset_parms for documentation.
Signature:
AskLinearIsetParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – Linear instance set feature identifier.
- edit (int) – This is an unused flag. It normally determines whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned. Set the value of this flag to integer value 1.
Returns: A Tuple
Return type: A tuple consisting of (numberInX,numberInY,distanceX,distanceY)
numberInX(str): Expression containing the number of instances in the X direction. This must be freed by calling UF_free.
numberInY(str): Expression containing the number of instances in the Y direction. This must be freed by calling UF_free.
distanceX(str): The distance between instances in the X direction. This must be freed by calling UF_free.
distanceY(str): The distance between instances in the Y direction. This must be freed by calling UF_free.
License requirements: None