NXOpen.UF.ModlGeneral.AskCircularIsetParms¶
-
ModlGeneral.
AskCircularIsetParms
()¶ Refer to UF_MODL_ask_circular_iset_parms for documentation.
Signature:
AskCircularIsetParms(featureObjId, edit)
Parameters: - featureObjId (Tag) – A feature object identifier
- edit (int) – This is an unused flag. It used to determine whether to return the right-hand side or both sides of an expression. Currently, both sides of an expression are returned.
Returns: A Tuple
Return type: A tuple consisting of (radius,number,angle)
radius(str): Iset radius. This must be freed by calling UF_free.
number(str): Number of instances. This must be freed by calling UF_free.
angle(str): Angle between instances. This must be freed by calling UF_free.
License requirements: None