NXOpen.UF.ModlFeatures.ExtractFace¶
-
ModlFeatures.
ExtractFace
()¶ Refer to UF_MODL_extract_face for documentation.
Signature:
ExtractFace(face, mode)
Parameters: - face (Tag) – Face to be extracted. Can be an occurrence.
- mode (int) – Type of extraction to perform. 0 = new_face should be the same type of face as the given face. 1 = new_face should be a cubic polynomial approximation of the given face. 2 = new_face should be a b-surface representation of the given face.
Returns: Sheet body created, this sheet is created in the work part.
Return type: License requirements: SOLIDS MODELING