NXOpen.UF.ModlFeatures.CreateVariableTaperFromEdges¶
-
ModlFeatures.
CreateVariableTaperFromEdges
()¶ Refer to UF_MODL_create_variable_taper_from_edges for documentation.
Signature:
CreateVariableTaperFromEdges(directionTag, angleStr, taperAllInstances, numEdges, edges, numPoints, points, angles, distTol, angleTol)
Parameters: - directionTag (Tag) – taper direction
- angleStr (str) – taper angle
- taperAllInstances (bool) – all instances or else just this one
- numEdges (int) – number of edges in array
- edges (list of Tag) – array of edges to taper
- numPoints (int) – number of points where angles are specified
- points (list of float) – coordinates of the points (size is 3*num_points)
- angles (list of str) – angle values or expressions at the points
- distTol (float) – distance tolerances
- angleTol (float) – angle tolerances
Returns: feature eid of created feature taper
Return type: License requirements: SOLIDS MODELING