NXOpen.UF.ModlFeatures.CreateTrueTaperFromEdges¶
-
ModlFeatures.
CreateTrueTaperFromEdges
()¶ Refer to UF_MODL_create_true_taper_from_edges for documentation.
Signature:
CreateTrueTaperFromEdges(directionTag, angleStr, taperAllInstances, numEdges, edges, distTol, angleTol)
Parameters: - directionTag (Tag) – taper direction
- angleStr (str) – taper angle
- taperAllInstances (bool) – If TRUE, all instances will be tapered. If FALSE, then just this instance is tapered.
- numEdges (int) – number of edges in array
- edges (list of Tag) – array of edges to taper
- distTol (float) – distance tolerances
- angleTol (float) – angle tolerances
Returns: feature eid of created feature taper
Return type: License requirements: SOLIDS MODELING