NXOpen.UF.ModlFeatures.CreateReparamSheet¶
-
ModlFeatures.
CreateReparamSheet
()¶ Refer to UF_MODL_create_reparam_sheet for documentation.
Signature:
CreateReparamSheet(projType, drvType, checkOverlap, numPrimary, primCvs, numCross, crosCvs, projVec, numFs, faces, tols)
Parameters: - projType (int) – Type of projection 0 = Use input vector 1 = Use driver surface normal
- drvType (int) – Type of drive 0 = Curves 1 = Face (B-surface type) 2 = Self-refit (B-surface type)
- checkOverlap (int) – Flag for controlling the overlap checking 0 = No 1 = Yes
- numPrimary (int) – Number of primary curves
- primCvs (list of Tag) – Object identifiers of the primary curves (face object identifier, if drv_typ != 0)
- numCross (int) – Number of cross curves
- crosCvs (list of Tag) – Object identifiers of the cross curves
- projVec (float) – Projection vector
- numFs (int) – Number of target faces
- faces (list of Tag) – Object identifiers of the target faces
- tols (list of float) – Tolerances: [0] = Distance tolerance in interior of surface [1] = Angular tolerance (in degrees) in interior of surface [2] = Outside edge distance tolerance [3] = Outside edge angular tolerance (in degrees) [4] = Projection size limit (0 - if no limit)
Returns: A Tuple
Return type: A tuple consisting of (newFace,tolAchieved)
newFace(Tag): Object identifier of the resultant face
tolAchieved(int): Flag indicating that the resultant face achieved the tolerance requirements. 0 = No 1 = Yes
License requirements: SOLIDS MODELING